hi,
may I know which is the widely used I2C mode among sm, fm, fm+, Hsm, Ufm in industry.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
may I know which is the widely used I2C mode among sm, fm, fm+, Hsm, Ufm in industry.
This all depends on the application, but in my experience working mostly with enterprise computing (e.g. servers) and communications infrastructure:
SM, Standard mode (100 kHz) is the most common simply because lower speeds are more reliable.
FM, Fast-mode (400 kHz) is also very common in architectures where all masters and slaves are made specifically for I2C, as opposed to a "bit-banging" approach.
FM+, Fast-mode+ (1MHz) is not very common but is starting to be adopted.
HSM, High-speed mode, is rare and I have never worked with it.
UFM, ultra-fast mode, is also very rare and is for uni-directional data transfer only.