Hello there
I have one question about datasheet.
When I check TPL0202 datasheet 17page, there is DPOT table.
In table, each RHW and RWL has maximu resistor is 100K ohm, is it right or typo?
I think it should be max 10K ohm,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there
I have one question about datasheet.
When I check TPL0202 datasheet 17page, there is DPOT table.
In table, each RHW and RWL has maximu resistor is 100K ohm, is it right or typo?
I think it should be max 10K ohm,
Yes, this is a typo.
The "-10" in TPL0202-10 stands for 10kOhm
Other places in the datasheet correctly say 10kOhm, but the decimal points in the table are in the incorrect place.