Hello,
The I2C signal from micro-controller(master) is connected to PCA9545A, and 4 slaves are connected to 4 individual channels in our design. We are able to communicate with individual slave by selecting respective channel(by writing to control register of PCA9545A). We are also able to communicate with multiple slave by selective multiple channels.
But we are facing issue when switching on all 4 channels and any one of slave is not powered on. In this scenario we are neither able to communicate any of slaves nor with control register of PCA9545A. We are getting NACK after Slave ID.
We are working at 3.3 V logic. We have probed the signal and found that signal level in is coming down to 1.5 V from 3.3 V in case all channel activated.
Please help us to find out the issue.
Regards
Pradeep