HI,
we are using the chip PCA9515B (as you can see on the enclosed file).
We've to do a mux for I2C.
U13 and U8 (AND ports) are useful to disable and/or enable the right i2c path (when I say path I mean comunication from gpioxx_x to M24C04 memory).
Considering that every SCL1 and SDA1 is shorted with M24C04 lines the question are:
1) Is the setup corrected?
2) Do I have to enable just one PCA9515B at time or do I have to keep every PCA9515B enabled?
I found that in case we keep enabled just one of the eight PCA9515B the gpioxx_x signal for SCL seems to experiment an high capacitance load (high rise time) while gpioxx_x signal for SDA seems to be stuck at one
Thanks and best regards.
Stefano Cumia