Hi,
Customer of mine is interested to use TCA9534A to expend more IO ports for processor
Could you advice the power consumption of this IC when all ports are functioning? (I could not find the power consumption in datasheet)
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer of mine is interested to use TCA9534A to expend more IO ports for processor
Could you advice the power consumption of this IC when all ports are functioning? (I could not find the power consumption in datasheet)
Thanks!
Hello,
This question is difficult to answer accurately due to the nature of the device. When a port is functioning, do you mean that it is at maximum loading capacity?
The datasheet specs quiescent current (ICC) through ground and VCC. If you assume that each of the 8 ports is at high level at maximum loading (10 mA), you will hit 8 x 10 = 80 mA through the VCC. Depending on your voltage (if you assume max of 5.5), you could see 0.08 * 5.5 = 0.44W.
Of course, if you don't load the pins at maximum load, or have a lower voltage, you will see a different dissipation figure.