Hello all,
I have a couple questions regarding the TCA8424. We are using the TCA8424EVM-038 plus the MSP430 Launchpad for evaluation.
1) Can this chip be programmed more than once, or can you only burn each chip once?
2) Are there any sample OTP files? This document ( http://www.ti.com/lit/an/scda013/scda013.pdf ) does not explain enough to create one from scratch.
3) The default values in the registers (un-programmed chip) make no sense for the 512 byte OTP. Are these chips expected to have a sample keyboard map and working HID descriptors at default, or are these expected to be programmed first before being functional? The datasheet ( http://www.ti.com/lit/ds/scds341/scds341.pdf ) leads me to believe that “The device also comes with a preprogrammed keyboard map that is compatible with most standard laptop/notebook keyboards”.
4) Is there a sample ACPI table entry for configuring this chip to work with Windows 8.1?
Thanks.