Hi,
I am looking for I2C Buffer/Repeater for 3.4MHz speed. The required bus voltage is 2.5V. May i know the part availability?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jonathan,
Thank you for the information.
I am also looking for a "Device" that should support the following requirement,
1.The Input of the device should be "Push-Pull/Logical signals(TTL/LVTTL)" compatible
2.The Output of the device should be an "Open drain" I2C compatible.
3.The Input & Output lines should be bidirectional with 2.5V compatible.
Kindly suggest us the best suitable part that meets the above requirement.
Hello Vishal,
I am going to assume you also need it to have 2 channels (for SDA and SCL), and relatively low speed (< 2mbps) is ok.
I'll loop the appropriate application engineer in to help with this.
I would starting by looking at the TXS0102
Hi Jonathan,
Kindly confirm TX0102 supports the below application.
Buffer Input Logic End – Push-Pull/Totem Pole (TTL/CMOS/LVTTL etc.)
Buffer Output Logic End – Open Drain (I2C Compactible)
Speed Grade – 100KHz or Any
Input side Voltage level – 2.5V
Output side Voltage level – 2.5V
Type – Bidirectional Level translator
We have connected Port A of TX0102 device to GPIO (Push-Pull/Totem Pole) of PIC Micro-controller which can generate I2C compactible waveform. Other End Port B will be interfaced to I2C Slave device with Open Drain Logic.