Hi,
I wanted to double check some Pull-Up resistor values I calculated for my I2C bus.
This board will only have 1 master 2 slaves, each contributing 5-10pF of load capacitance.
I am unsure on exactly how the total bus capacitance is calculated, but I performed two calculations.
The first was done if total bus capacitance is calculated by adding both SDA and SCL pins as if they were in parallel, and the value I got was 7kOhms. Very reasonable.
If the total was calculated per lane (one for SDA and SCL), then I got 14.1kOhms of course. This seemed reasonable, but larger than I've seen so far.
My guess is the lower one is safer either way, but I wanted to double-check before I finalized anything and make sure I am correctly calculating total bus capacitance.
Thanks!
Luis Cordova