Hi
I have board with PCF8575
When I use it as output all the 16 port working OK
When I want to use PCF8575 as Input just
half of the PCF8575 is working - P0
P1 - the second port not responding to the input port
When I check with fluke the voltage on the pin - I saw the voltage on the pin rising up - to 3.3V\5V
I have isolation on the ports
What can be the problem
one port (P0) working
the second (P2) not
Your help needed
Mayer