Hi all.
I have two questions about the internal circuit of PCA9544.
1. I use this device the following case, is this device maintained without breakege?
・Vcc=0, INT0_4=5V, A0_2=5V
I am concerned that this device be latch up breakege,
but I think this device has the protection from Input pin absolute voltage range.
2. Does this device have parasitic diode in the internal route between input pin and Vcc?
Best Regards,
Sho