Hi,
We are designing a P82B96 based I2C prototype for low frequency (40kHz) long distance (upto 300m) master-slave communication - smart energy meter application. The pull-up voltage on the Long Distance Transmit sides (Tx,Ty,Rx,Ry) is 12V - powered using a 12V 5A SMPS. We are much concerned about the voltage ripples/Noise on the SMPS output. The SMPS datasheet indicate 100mV noise at 45kHz switching frequency.
Can someone please let us know if the above SMPS can safely be used with P82B96 for I2C communication at 40kHz Bus Clock Speed without any interference? Also, please suggest if there is a better way to suppress the noise from SMPS.
Also, do we need to connect a current limiting resistor on P82B96 Vcc pin when connecting it to 12V line?
Regards,
Ravi