Hi,
Can we have some reference value of tr/tf of output signal for SN74LVC8T245?
It should be OK with the condition of test circuit in datasheet and should not be guaranteed value.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can we have some reference value of tr/tf of output signal for SN74LVC8T245?
It should be OK with the condition of test circuit in datasheet and should not be guaranteed value.
Best Regards,
The output rise and fall times depend on the VCC and the output load. They will vary accordingly.
LVC device will have approximately a 2ns rise and fall time at 3.3V into a 30pf /500ohm load. If you are driving a typical Cmos input the rise and fall will be faster. approximately 1ns.
Hi Chris-san,
Thank you for your information.
As you said the output rise and fall time will vary depend on Vcc and the output load, but the reference value you provided will be helpful for customer.
Best Regards,
Sonoki
Hi Chris,
If the load is a TTL input, VccB=5V, VccA=2.5V, data is from A port to B port, what tr/tf should be?
Best,
Mark