This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC fan-out and applications question

Other Parts Discussed in Thread: SN74AVCH24T245

I am trying to find what the fan-out for the sn74avch24t245 is.

I understand it is a bus transciever, but I intend to use it as a fan-out buffer and level shifter.

Problem:

  • I will be level shifting (6) control signals from 2.5V to 1.8V and distributing to 13 ASIC's (these signals will always flow from the 2V5 to 1V8 side).
  • Each ASIC digital input has a load of approximately 10pF + there are several interconnects and other items which will add parasitics.
  • At this point I am considering doing the following: