Hi!
In my design, the input device to the TXS0104E has a VOL max value of 0.4V (pg. 3). I am using 1.8V for VCCA and 3.3V for VCCB.
After checking the TXS0104 datasheet, the VIL max value is shown as "0.15V". However, in comparison, the VIL max value shown in the TXB0104 datasheet is "VCCI x 0.35 V".
I'm wondering if there is a typo in the TXS0104 datasheet and the VIL max value should be "VCCI x 0.15 V" instead of "0.15V"?
This makes quite a difference for my design: VIL= 3.3 x 0.15 = 0.495V versus VIL = 0.15V for VOL max = 0.4V.
Thanks for your help in advance!
James