I am using a SN74ALVC164245DGGR for level translating ( 3.3V-5V) data bus in my application.
1. The datasheet mention that “The input circuitry on both A and B ports always is active and must have a logic HIGH or LOW level applied to prevent excess ICC and ICCZ.”
Does this mean that a Pull-up or pull-down on data bus is essential if this level shifter is used ?
2. Port A is connected to 3.3V microcontroller; Port B is connecting to 5V asynchronous memory.
Initially direction control signal (DIR) is set such that the data direction is form port B to A (memory to microcontroller). Oscilloscope digital probes are connected at port B, the probed data is 0xF0F0.
Now the direction control signal inverted and the direction is from A to B. no data is emitted from micro-controller which at Port B side.
Till the time some data is emitted from micro-controller the data 0xF0F0 remains latched on portB.
Does this level shifter have a bus hold circuitry implemented?