Hi Team,
Please give me a help about TXS0102 operation.
Our customer uses TXS0102 x2 in the SPI bus line. They observes total more than 40mA in the 3.3V power line only for these 2 devices. It seems 40mA is too high for these devices.
What is the nominal current consumption for this device when it is operating successfully, when having input and output signal ?
[Condition]
- VCCA=3.3V, VCCB=5.0V
- Connected devices have CMOS Input/Output
Best Regards,
Kawai