Hi,
One of my customer wants to use device SN74AVC16T245-Q1, they are having some clarifications, kindly help on this.
Q1. Will this device suitable to be used in GMII (Gigabit Ethernet interface)?
MAC side is 1.8V IO,the PHY chip is 2.5V IO. Will this level translator suits this application?
Q2. Will there be any skew among the 16 outputs?
The Tphl & Tplh are given some range values about 0.5 to 7.5 ns. They want to have a clarification that the output1 to 16 will have same propagation delay values or it varies from port to port?
Regards,
Aravind