Hello,
I'm trying to interface an ASIC with a FPGA. The voltage level on the FPGA side is 3.3V and in the ASIC side is 1.2V. There is a clock signal between them of 100MHz used to synchronize the data transmission. I would like to use the SN74AVC32 to convert logic levels from 3.3V to 1.2V and vice versa, but I'm not sure if it will work properly at 100MHz.
Best regards,
Jordi