This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Yaita-san
Thanks for using our part, here is the feedback for your concerns. any unclear, please let me know.
1) Yes, you are right, the TXS0108E does have the integrated pull up reisitor, so, if hold "H" needs, no externall pull-up resistor need to add.
2) to hold "L" level , it is a little complicated, could you please clarify the detail application scenario for the hold "L" ?
For example, when power on, what the detail required, or when power off, what the detail required, or when normal working, what the detail required etc. also will it transfer the bi-directional signal or the uni-direction signal? and the transfered signal is open drain or push pull ?
The main reason is, if it is the bi-directional signal, you can not add the stronger pull down resistor, in case you output VOH has much drop.
While , this weaker pull down can not pull the output to low when the driver stops to drive the TXS0108E and the TXS0108E just has the High output before.
That is the reason I say it is a little complicate to hold "L" level, whether it can be implement or not, it based on the application itself.
BR
Junjie
Hi, Yaita,
Yes, what your understanding is correct. I just have the sample on hand and did some test and then provide the feedback to you.
1. Since you need have the "L" at the 5V side (B side) when power-up sequence, I suggest you have below design.
2. Put the stronger pull down at the input 3.3V side (A side), less than 1K. like 500ohm, while it needs you check your MCU, whether it has higher current drive capability, because dirving 500ohm pull down to high , it needs at least 3.3/500 =6.6mA. if 1K, it needs 3.3mA.
3. Put the weak pull down resistor at the output 5V side(B side), because, for our part, if one of Vcc is about 0V, the IO will be in high-Z state, so when at the power up duration, the A side low can not be transfered to B side. so you need to put the weak pull down at the B side before the power up sequence finish. like 150K or 200K.
4. While , you know power up duration and power down duration , no part can make sure the transfer function. so for making sure no unexcepted glitch at power up or power down. so suggest to have the VccB power on and power down firstly since your B side is connectted to the receiver.
any unclear, please let me know.
BR
junjie