Hello,
is there a bidirectional level translator with Vcc = 2.5 - 3.3 V, static Icc < 10 uA able to translate open drain pull up ports, VpullA = Vcc, VpullB = 2 - 5,5 V. The speed of the interface is 100 KHz and less.
Thanks
Martin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Wei,
thanks for your suggestion but I think this part is not suitable as it has high level input voltage recommended to max Vcci.I need it to be max 5,5 for port B.
Thanks
Martin