Hello,
I am using SN74AVC8T245PWR level translator to interface with GSM. i have given 2.8 to VCCA and 3.3 to VCCB,i have connected channel A3 of SN74AVC8T245PWR IC to GSM reset pin and GSM reset pin has internal pull up. After power on the level translator A3 channel voltage level is supposed to be high because of GSM internal pull up but it is driving A3 channel to low.
I have ordered sample IC from TI website and it works fine and voltage at that pin is high but i ordered IC through digikey and those IC's r driving that pin low. Kindly tell us that what is the difference between sample IC and ordered IC,why there is funtionality difference between both?