Hi TI and forum
I need a level converter to converter a 5V signal to a 3.3V signal. The signal is a simple rectangular 5V pulse of 10 microseconds duration. Once converted to 3.3 volts this signal will edge-trigger a hardware interrupt on one of the GIO pins of the TI Hercules LaunchPad microcontroller evaluation board. What would be a good choice for the level converter? I need a level converter that can be hand soldered. Also, the Hercules board is powered by a 5V source. Can the recommended level converter be powered by the 5V source to the Hercules LaunchPad?
Thank you,
Dan