Hi,
I have to use a level shifter for my parallel camera interface. I am using an MCU with 3.3V level and the OV5640 camera sensor uses 1.8V. I have setup a small prototype. In this prototype my 3.3V MCU sets a GPIO HIGH and LOW every second. This is connected to Pin 11 of LSF0108. I pulled pin 20 up on 3.3V with a 200k resistor. I connected pin 19 to 3.3V. On the other side I connected pin 1 to GND and pin 2 to 1.8V (which is created from a voltage divider from the 3.3V).
Which a scope I measure pin 11 which shows the signal oscillating from 0V to 3.3V and back every second. Measuring pin 10, which should give me a 1.8V HIGH signal (as I understand it) just gives me 2.5V.
I don't understand why that happens? I have tried with a Dual Power Supply, delivering 3.3V and 1.8V sharing GND. The same result, I don't think it's the voltage divider. I also pulled up pin 11 and 10 with different resistor values (47, 100, 220, 330, 1K, 10K, etc) - the voltage level changes between 2.3V and 2.5V.
I have screenshots from my scope and made a picture of my breadboard, but I am not able to post them here in this post as far as I know?
Any help would be appreciated.
Thanks,
Phillip