Hi,
When VCC=floating, A or B pin=3.3V, what voltage can I see in VCC?
When A or B pin=3.3V, can I see some voltage xxxmV in VCC due to internal block like internal pull-up?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When VCC=floating, A or B pin=3.3V, what voltage can I see in VCC?
When A or B pin=3.3V, can I see some voltage xxxmV in VCC due to internal block like internal pull-up?
Thanks.
David,
I am trying to get a better understanding of what you are asking. In the application the SN74AVC4T245 is used for, when and why would you need to check the Vcc floating value?
Applying a voltage between 1.2 V and 3.6 V to Vcc is essential for the device to function properly. If you apply 3.3 V to either the A or B port and leave the Vcc floating, you can check to see if there is a xxxmV on the Vcc pins, but the device loses function. Is there a particular reason why the floating voltage value would be important to you/your customer?
Regards,
Jared