Hi,
Could you provide us the additive jitter @fclk=66MHz for SN74AUP1T58 ?
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you provide us the additive jitter @fclk=66MHz for SN74AUP1T58 ?
Best Regards,
Kato
Kato-San,
We dont have this spec for the SN74AUP1T58. The closest spec will be a propagation delay skew.
Parts like LMK00105, which specifically distrubute the clock signals with low jitter,will have jitter charactrized at different frequencies. This will also be an electrical spec.
If you explain your application and need for this spec, I can assist you further.
Thanks
Hi Jennifer -san,
Thank you for the reply. We have not information for this spec. we are considering replacing clock devices for cost reduction.
Best Regards,
Kato
Hi Kato-san
The magnitude of the time difference between the high-to-low (tPHL) and the low-to-high (tPLH) propagation delays when a single switching input causes one or more outputs to switch is the "pulse skew". There are several skew specifications, this is the one that I feel might be applicable for your application. Since both tPHL and tPLH are same for this part, we have to assume that the delay is insignificant.
Unfortunately, only the clock buffers will have the jitter specifications. If required, I can check for cost effective options in that group.
Thanks