I'm using a TXB0102 and on my first round of boards I directly tied OE to VCCA. When I wiggle the B pins, the A pins do not wiggle. Could this be because OE is ramping with VCCA?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using a TXB0102 and on my first round of boards I directly tied OE to VCCA. When I wiggle the B pins, the A pins do not wiggle. Could this be because OE is ramping with VCCA?
Thanks,
Hi Jennifer,
I did some more digging and it turns out OE wasn't my problem at all! My input signals on the B side were only toggling between 0-2V. Injecting 5V caused the TXB's output to go high.
The weird thing is when I depopulated the TXB from the board my input signals went back up to 5V. The signals are generated by an optical encoder powered by 5V:
Do you know why the TXB would be clamping the signal to 2V? Could the input/output of the two devices be incompatible?