I’m now verifying the LSF0108 on my board to check if it can support 50MHz. Now it can work. But the waveform is a little strange.
Here is the schematic.
I used the pull up resistor based on the table in datasheet. The behavior is different for different signal.
- 3.3V Pullup 1K, 1.8V Pull up 510ohm
- Data is OK
- 50M CLK cannot pass from 1.8V to 3.3V
- CMD is only 2.0V when the CMD pass from 1.8V to 3.3V.
- 3.3V Pullup 1K, 1.8V pull up 180ohm for CMD. It is OK
- No 3.3V Pullup, 1.8V pull up 680ohm for CLK. Clk is single direction signal and only pass from 1.8V to 3.3V side. The CLK is only 2.0V on 3.3V side. But the card can work. When I reduce the 1.8V pull up to 180ohm, the low level of the CLK on both side increase to 1V. I cannot get a suitable configuration for the clock. Do you know why?