Hi,
I am trying to use the TXB0106 as level shifter on an SDIO-bus between a 3.3V host and a 1.8V peripheral. I would like to use a pull-up resistor on the cmd line for example, but it seems as if the circuit doesn't work with that. I put a 56k pull-up to 1.8V on one of the 1.8V side input/outputs, but if I then measure the voltage at the pin it is not 1.8V, but more like 0.3V. Shouldn't it be possible to define a logic high level like that with the TXB0106?