Dear experts,
Is it possible to use for example the LSF0204 for an SPI application where the i have a 3.3V microcontroller and a 5V SPI device. On the 5V side i have a pull up resistor with 3.3kOhm. The clock frequency is at max. 40MHz. Is there any equation to calculate the maximum pull up resistor?
Best regards