We have two digital sources which are 5V and 2V respectively and want to translate both of them to 3.3V and have them be exported through two channels and LSF will be a wonderful choice. But a further question is if the A port input is 2V can I still set Vref(A) as 1.8V since 1.8V is a much commoner voltage than 2V, Thanks.