Hi,
There are two orderable devices, 74LVC8T245RHLRG4 and SN74LVC8T245RHLR - are there any differences between them functionally, packaging, material ,etc.?
Cheers
Calum
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There are two orderable devices, 74LVC8T245RHLRG4 and SN74LVC8T245RHLR - are there any differences between them functionally, packaging, material ,etc.?
Cheers
Calum
Calum,
No difference. Click on the QUALITY tab: www.ti.com/product/SN74LVC8T245/quality , then View . You'll see the STD non-G4 part was converted to RoHS in 2004, so prior to this date, it was NOT RoHS compliant. If you have parts made prior to 2004, they would not be Pb-free.
Search part number | TI part number | Part number type | RoHS status | RoHS conversion date1 | Green status | Green conversion date1 | Package | pins | Assembly site | Lead/ball finish | MSL/reflow ratings | Mass (mg) |
---|---|---|---|---|---|---|---|---|---|---|---|
SN74LVC8T245RHLR | 74LVC8T245RHLRG4 | Pb-Free | Y | 01-Sep-2004 (DC 0436) | Y | 01-Sep-2004 (DC 0436) | RHL | 24 | TI MALAYSIA A/T | CU NIPDAU | Level-2-260C-1 YEAR | 51.200000 |
SN74LVC8T245RHLR | SN74LVC8T245RHLR | Std | Y | 01-Sep-2004 (DC 0436) | Y | 01-Sep-2004 (DC 0436) | RHL | 24 | TI MALAYSIA A/T | CU NIPDAU | Level-2-260C-1 YEAR | 51.200000 |