Hi Team
This is South China AFAE Randy who support Zhuzhou (China high speed train design), my customer is using many logic devices like SN74LVC8T245, and recently we need to review the design for initial status for each device.
8T245 is started at 1.65V with high level voltage at 1.07V, so I’m wondering what’s the status below 1.65V? If I give 8T245 a 1.2V supply voltage with 0.65*1.2V input signal, does 8T245 output a high level voltage?
Or can you tell me the lowest startup voltage for this device? Is the high level threshold also 0.65*Vcc at this moment? Thanks.