I am reading this datasheet for this part and I have a few questions:
http://www.ti.com/lit/ds/symlink/txb0108.pdf
1) Can this part drive a 1 mA load?
2) Can this part sink an 8 mA load? I would like to connect this part to an FPGA with an 8 mA output driver on the output pins.
3) Are the ports completely independent meaning that port A1 can level shift from 3.3V to 5V when port B2 level shifts from 5V to 3.3V?
Thank you.