Hi, We are using CD40109B for our same production boards for over 20 years. The IC is enabled at pin2,7,9,15 by 12VDC through (4.7kohm + 15kohm) serial resistors. VDD is at 15VDC. Recently we saw quite often that the voltage at CD40109B enable pin (2,7,9,15) dropped to 0 ~ 3V, while the driving voltage from the system bus is still remaining at 12VDC. I either have to replace the IC or decrease the current limit resistor value from 15kohm to 6kohm with jumper wires, resistor pot. The system is at room temperature testing cage. It runs the final test for a few weeks, and then suddenly a lot of boards failed near at the same time.
I would like to know how much current needed to enable CD40109B under normal condition. According to my understanding from the data sheet, it is in ~ 1uA range for each IC. Our system bus can provide up to 2.6mA driving 10 same kinds of boards at the same time. What could cause the failure of CD40109B? How can I prevent the damage happened again? Should I change the design how we enable this IC?
Thank you! Jing