Dear Sirs
I follow the LSF0102 datasheet Rpu setting but there is some issue in Voltage_Low.
- For the following schmatic oniginal setting: B1 Voltage_Low 1.31V, Voltage_High=3.43V
- remove R5: B1 Voltage_Low 0.615V Voltage_High=3.33V
- remove R5/R12, B1Voltage_Low -0.134V Voltage_High=1.90V
- remove R5, R12 change to 1Kohm, B1Voltage_Low 0.184V Voltage_High=3.6V
Could you help me about the Rpu setting issue?
BRS
Nat