Hello Team,
This is similar question to my previous question in the following URL.
https://e2e.ti.com/support/interface/etc_interface/f/391/p/425052/1519517#1519517
Could you please tell me about below questions ?
[Q1]
Do SN74AVC4T774 may have leak voltage from VCCA to VCCB or to other pins when VCCA is only applied ?
[Q2]
Do SN74AVC4T774 may have leak voltage from VCCB to VCCA or to other pins when VCCB is only applied ?
[Q3]
Do SN74AVC4T774 may have leak voltage from /OE to VCCA/VCCB or to other pins when /OE is only applied ?
I believe there would be no voltage leak from each pin to other pins. For power up sequence, either VCCA or VCCB can be applied first, however, it requires to keep /OE pin High until VCCA and VCCB is fully ramped and stable.
Best Regards,
Kawai