Hi,
I am using TXB0104 for shifting signals from VCCB = 3V3 to VCCA = 2V8.
While reading the datasheet there came up two questions.
1. Is it ok to connect a 10k resistor between VCCA and OE? I want to have the output permanently enabled and I've heard that it isn't so good to connect VCC and OE directly.
2. In the Datasheet txb0104-q1.pdf p.14 section 9.2, there is shown a typical application with a resistor between OE and ground. What is the dimension of this resistor? I think it is the pull-down to set the OE to low, but when I need my OE always on high, I think I can leave him out.
Am I correct?
So I just need the resistor from question1, right?
Thannks alot for your help and tipps.
Best Regards
Jerrry