Hello,
In the datasheet of SN74AVCA164245 page 1, there is the discription as below.
"Dynamic Drive Capability Is Equivalent to Standard Outputs With IOH and IOL of ±24 mA at 2.5-V VCC"
Hoever, in the EC table on the page 5, the IOH and the IOL is +/-12mA at the condition of 2.4V to 2.7V VCCO.
Could you please let me know his reason? Which are values correct?
Best Regards,
Ryuji Asaka