• Not Answered

MAX232 overheat problem

Dear All,

Please don’t take this mail as a beginner mail. I have really a serious problem that turns my twelve months product design to a waste.

I designed a an RS232 interface board and used MAX232CWE+  16 wide SOIC

I used 1uF/50V SMD Case B Aluminum Electrolytic capacitors for MAX232. I use a generic 100nF SMD capacitor as a decoupler of MAX232.

You can see my sch. and layout parts below;

Here is my problem,

When I connected my system to a PC serial port via an RS232 cable  (19200 baud and no parity, etc);

1.       There is no problem first. System is communicating correctly.

2.       I started to disconnect  and connect  the serial port periodically while my finger was on the MAX232 to measure the heating  J

3.       In some way MAX232 is starting to overheat and the serial line is starting to not working.

4.       If I close my system while MAX232 is heating, waits MAX232 get cold for nearly 1 minute and plug the system again there is no problem. MAX232 is working well.

5.       If I don’t close the system, MAX232 is damaged because of the heating.

6.       I dumped the problem with an oscilloscope. When I send some bytes to the system via a PC I should see nearly 12,13V if there is no problem but when the IC is damaged, I see only 1V at the R1IN pin (13. Pin) of MAX232. So I’m sure that MAX232 R1IN pin was collapsed  the PC transmit signal. Please note that none of five capacitors for MAX232 was not damaged or heating up.

7.       I changed the MAX232 IC and all of the rouitine is starting again. I did this nearly 10 times J

8.       Please also note that I double checked the capacitors polarity. There is no  problem for all

9.       In maxim site It tells about an ERRATA for MAX232CWE+( Product Change Notice 801-ERRATA) ; However I couldn’t find this document. I suspected that this IC has a BUG that I encountered

10.   I’ve searched the internet for 1 week and there are same problems but all of explanations are about look at the directions of the caps, etc.

11.   I found a forum thread on TI forums below and a person named David connected a 20 ohm series to MAX232 VCC and solved his problem. It is not a good but may be a reasonable solution

http://e2e.ti.com/support/interface/etc_interface/f/392/t/123614.aspx

12.   I know there is a TI employee could check my problem in detail. If you do I’ll be very glad

Waiting for your urgent reply

Ertan

29 Replies

  • In reply to saltan:

    Saltan,

    I have tried to get the MAX232 to overheat but I was not successful. Can you return a couple devices to your distributor as defective for failure analysis. It would be good to return samples that have the overheat issue but still work after cooling off. Also return some that are permanently damaged (don't work when cool).

    The C3 capacitor can be placed in either location for either device. It does not affect the charge pump action.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

  • In reply to Ron Michallick:

    Hi,

    I've connected the C8 negative pin to VCC and measured the VCC, V+, V- for damaged and not damaged IC at run time. Please see below 
    NOT DAMAGED MAX232 ON BOARD 
    VCC: 5.09V 
    V+ : 9.3V 
    V- : -8.71V 
    Some Pins of MAX232: Squarewave signals 
    Heating: NO 
    DAMAGED MAX232 ON BOARD 
    VCC: 5.09V 
    V+ : 4.3V 
    V- : 1.2V 
    Some Pins of MAX232: NO Squarewave signals 
    Heating: LIKE HELL 

    I'm pretty sure that the VCC is stable

  • In reply to saltan:

    Dear All,

    Do you think that the below switching freqencies are normal   

    MAXIM MAX232CWE+  : nearly 600KHz at pin 3

    TI MAX232 : nearly 45KHz at pin 3

    I read to many things on the net about charge pump capacitors. In short;

    - if you use fast switching you need lower capacitance

    - if you need low switching you need higher capacitance

    From this point of view, capacitors suggestions for  "600KHz and 45 Khz" are same and 1uF. for both TI and MAXIM ICs ???

    Do you have any comments for switching frequencies and capacitor selection

  • In reply to saltan:

    Saltan,

    45kHz is too low. I do not have data on hand for the nominal frequency of the charge pump. I will check some samples this week.
    It takes a lot of current to pull the V- pin positive. There is a Schottky diode to ground on the V- pin.

    On devices that overheat but are not destroyed, is the V- pin also positive? It seems that the MAX232 is latching up.
    Other users who added a VCC resistor may have prevented latch up by limiting the (SCR) hold current so the latch is unsustainable.

    I do not know where the trigger for the latch originates, but the trigger is certainly external to the device.

    Have you considered upgrading to the MAX202? It is the same cost and is a drop in alternative to the MAX232. Both device have the same function, but the internal schematics are very different.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

  • In reply to Ron Michallick:

    Dear Ron,

    Thanks for your answer. Please see below for my answers;

    45kHz is too low.

    I see nearly 45kHz with an oscilloscope. 

    I do not have data on hand for the nominal frequency of the charge pump. I will check some samples this week.

    It takes a lot of current to pull the V- pin positive. There is a Schottky diode to ground on the V- pin.

    On devices that overheat but are not destroyed, is the V- pin also positive?

    Yes V- pin also positive for both TI, or MAXIM ICs. I tried them on the same PCB.

    It seems that the MAX232 is latching up. 
    Other users who added a VCC resistor may have prevented latch up by limiting the (SCR) hold current so the latch is unsustainable.

    I do not know where the trigger for the latch originates, but the trigger is certainly external to the device.

    Have you considered upgrading to the MAX202? It is the same cost and is a drop in alternative to the MAX232. Both device have the same function, but the internal schematics are very different.

    I do not use MAX202 But I can. Pins are ok but footprints are a little different. I may use it.

  • In reply to saltan:

    Saltan,

    You are correct, the MAX232 does run near 45kHz. It is the MAX202 and entire MAX/TRS32xx series that runs over 100kHz.

    The V- should always be negative in operation. I tried forcing V- positive (up to 1Amp), but it ran normally once, I stopped the abuse.

    I have not been able to get any MAX232 to latch-up (overheat) in the several times I have tried. Please try the MAX202 and let me know the result.

     

     

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

  • Dear Ertan Bey,

    When you design the circuit you didn't consider ESD considerations.  am sure that the shield of DB9 its connected direct to GND or not connected. I always use 100 ohm serial,100nF to GND  for each pin from DB9 to IC. 1 uF capacitors use as multilayer ceramic low ESD type instead Tantalum. Less space, lower price better performance.

    When you do this please share the results with us.

    BTW - There in mounting hole on trace to Pin# 8 of DB9 I hope its not plated hole and you have short to GND

    Sevgiler,

    Haim Rodrik - CEO/CTO

    jTrack M2M Tellocation Systems LLC

  • Note: Between the DB9 shield to board's GND connect via Ferrite bead parallel 1000pF/2kV 0805 capacitor.

      if you need more assistance feel free to use rodrik5000

  • In reply to Haim Rodrik:

    I have reached this forum in search for a solution for the same latch-up situation.

    In my case I think I have found the scenario that causes the latch-up - every time the analog side RS232 pins of the chip are connected to a powered serial port (e.g. connecting a board with the MAX232 to a running PC's serial port) without power applied to it's power pins (i.e. the board not powered), once I apply +5V to the chip it immediately enters the latch-up condition. I have narrowed this to the TxD input - because it's driven with a negative voltage (negative idle voltage on RS232 line), the combination of rising VCC and negative input on TxD causes in my opinion the latch-up condition. This seems like a bug of these chips related to the silicon implementation.

    Can TI tech support check this analysis and try t simulate it too?