Hi
I have a problem with a board with a MAX3232 device. What happens is if the MAX3232 is powered with a device (in this case a standard PC serialport) connected to the RX Input the charge pump doesn't appear to work. If you remove the connection and reconnect everything is fine and if you power the MAX3232 before connecting the PC everything is ok. It is only if there is -12V on the RX input when the MAX3232 is powered up that this happens. I have used these devices in plenty other designs over the years with no issues. On the board the MAX3232 is connected to a NXP LPC1752 Cortex-M3 processor.
Has anybody any idea of what could cause this behaviour?
Thanks
Ian
Hello Ian,
This effect has not been reported before. Can you measure the voltages on the device pins when this anomaly occurs? Use an oscilloscope to see if there is any clocking. The pin voltages will be helpful in determining the root cause.
Does this happen on more than one MAX3232 device? Is it a new design?
Regards,Ron Michallick
Regards,Ronald MichallickLinear Applications
TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).