I work an existing schema, the MAX232 is connected :
the inputs (10 and 11) were connected together to the same pin of the Controllers.
the outputs (7 and 14) were connected together to the same pin of the receiver.
my question is :
- The RS232 output working properly?
- What is the role of connected the 2 output together ?
cordially