This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Couldn't link with ET1100

Part Number: DP83822I

Hi Sirs,

Sorry to bother you.

As title, DP83822 couldn't link with ET1100

Actually we use TLK110 before and could be work, but change to DP83822 is fail.

The boot strap already setting, the 25MHz CLK ready too.

We think schematic is OK, but could you help double confirm again?

ET1100 schematic

DP83822I schematic:

4 Replies

  • Hi Sirs,

    Sorry for push, any update on this ? 

    Thanks!!

  • In reply to Shu-Cheng LIN:

    Hi Sirs,

    Sorry for push, any update on this ? 

    Thanks!!

  • In reply to Shu-Cheng LIN:

    Hi Sirs,

    Update state.

    We found RX_CLK only sent 1.25MHz? From datasheet spec is 25MHz on 100Mbps MII  Mode, so should be  2.5MHz on 10Mbps.

    Am i wrong?? 

    Could you share experience for us?

  • In reply to Shu-Cheng LIN:

    Hello Shu-Cheng,

    What are the problem symptoms?
    When you say that the PHY doesn't work with ET1100, does the PHY power-up and link with a link partner?
    Can you provide the the register values of 0x00, 0x01, 0x09, 0x0A, 0x0B, 0x10, 0x11, 0x016, 0x017, 0x018, 0x019 after power-up and connection with link partner? Please read register 0x01 two times, all other registers can be read once.
    In your schematics, there is a separate "Strap" section but PHY0_Link and PHY0_ACT have extra resistors connected on the last photo, R194 and R168. Can you tell me why those resistors were added?

    -Regards,
    Aniruddha

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.