I have a question regarding timestamping accuracy/resolution of the part. What resolution can I expect to get when reading the timestamp via the PTP_CTL PTP_RD_CLK method or via the gpio event timestamping functionality? We have tried both of these methods triggered via a GPS pulse per second output that is accurate to (at worst) 100 ns of UTC. When corrected for frequency, we are only seeing a resolution of +/- roughly 65 us with spikes in these values into the hundreds of microseconds/low milliseconds.