Hi all
Would you mind if we ask DP83867IR?
Please refer to the following attachment file.
20170327_DP83867_RegisterSetting.pdf
Especially, we have a question about Basic Mode Control Register(BMCR), bit "Speed Select (Bits 6, 13)".
When we would like to use 1000Mbps, are bit6=1 and bit13=0 correct setting?(the datasheet shows 10 = 1000 Mbps)
Kind regards,
Hirotaka Matsumoto