This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83865: What PHYTER is best suited for Extending reach of Optical gigabit Ethernet?

Part Number: DP83865
Other Parts Discussed in Thread: DP83867E

I need a reach extender for FO based gigabit Ethernet.  Need an IC or IC set that can connect with an SFP transceiver on each side to receive and repeat Ethernet packets.  I want to concatenate multiple units for a longer transmission reach.

  • Hi Bradley,

    The DP83867E can be used with SGMII to connect to an SFP. You would need to have two DP83867 devices connected together through because the MDI side does not support fiber. You would need to have both DP83867 PHYs MDI pins (channel A-D) connected through a transformer.

    Kind regards,
    Ross