This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/DP83822HF: DP83822HF FX Not working.

Part Number: DP83822HF

Tool/software: Linux

Hi.

I'm using AM572x custom board

and, DP 83822HF is connected to RPU2 ETH0/ETH1

I have question.

Q1. GENCFG(0x465) "phy_read" value is invalid.

        The value does not changed when i set  "phy_write(phydev, 0x465, 0x1);"

==== DP83822HF_read_status 761===
BMCR(0x0): 0x3100
BMSR(0x1): 0x7849
PHYIDR1(0x2): 0x2000
PHYIDR2(0x3): 0xa240
CR1(0x9): 0x0
CR2(0xa): 0x4100
PHYSCR(0x11): 0x4100
RCSR(0x17): 0x41
LEDCR(0x18): 0x400
PHYCR(0x19): 0x21
GENCFG(0x465): 0xffffffea
=================

Q2. DP83822HF Reg value is correct.
       But, I don't know why FX not working.

Best Regards

John

  • Hi John,

    The register in question, 0x465, is an extended register and as such has a different access method than the other registers in your status dump.

    I am not sure how the AM572x MDIO access is created, but you will likely have to use the indirect access method described in section "8.4.2.5 Read (No Post Increment) Operation" of the DP83822HF datasheet.

    I am not sure what your question is in Q2. Can you elaborate?

    Best Regards,

    Rob Rodrigues

    EFL (Ethernet & FPD Link) Applications Engineer

  • In reply to Rob Rodrigues:

    Hi,

    Thank you for your reply.

    I need to operate DP83822HF in FX mode.


    Q2. I wrote 0x4000 to the CR register, but it didn't work.
    Are there any other settings besides FX_EN?


    Best Regard,
    John
  • In reply to Yohan Kim:

    Hi John,

    You should only have to set bit[14] of the register address 0xA to get FX mode enabled. You said you write 0x4000, but there is a reserved field that should NOT be modified.

    Please read the default value of 0xA register, then set bit[14] and do not change any of the other bits.

    Could you also provide a schematic of only your PHY?

    Best Regards,

    Rob Rodrigues

    EFL (Ethernet & FPD Link) Applications Engineer

  • In reply to Rob Rodrigues:

    Hi Rodrigues,

    I am already set bit[14] and do not change any of the other bits.

     

    CR2 Reg val is 0x4100.

    Are there any other settings besides FX_EN?

    ------------------------------ reg set code ------------------------------------------------

    val = phy_read(phydev, 0xA);

    val |= 0x4000;

    phy_write(phydev, 0xA, val);

    -------------------------------------------------------------------------------------------------

    Schematic file.

    PRU2_1_FX.PDF

    ==== DP83822HF_read_status 761===

    BMCR(0x0): 0x3100

    BMSR(0x1): 0x7849

    PHYIDR1(0x2): 0x2000

    PHYIDR2(0x3): 0xa240

    CR1(0x9): 0x0

    CR2(0xa): 0x4100

    PHYSCR(0x11): 0x4100

    RCSR(0x17): 0x41

    LEDCR(0x18): 0x400

    PHYCR(0x19): 0x21

    GENCFG(0x465): 0xffffffea

    =================

    Best Regard,

    John

  • In reply to Yohan Kim:

    Hi John,

    It looks like you are setting register 0xA properly but I do have 1 concern. Your schematic shows a bead and a 10nF cap only for the PHY. Please implement the cap decades required by the DP83822 datasheet.

    It may be possible that as you switch from TX to FX mode, the PHY is starving for current and causing a failue.

    Can you also strap the PHY into FX mode rather than change the register? You could also remove the bead from your design and replace it with a 0ohm resistor.

    Best Regards,

    Rob Rodrigues

    EFL (Ethernet & FPD Link) Applications Engineer

  • In reply to Rob Rodrigues:

    Hi Rodrigues,

    I tried both(FX Boot strap / DP83822 Datasheet guide).

    but, FX Mode is not working.

    I have question.

    how to configuration 'PECL termination resistance' of DP83822HF

     

    Best Regards,

    John

  • In reply to Yohan Kim:

    Hi John,

    The DP83822IF and DP83822HF are both current mode line drivers.
    They are not PECL and thus have different biasing.
    From your attached schematic it looks like you are not properly biasing the PHY.
    Please refer to page 89 in the datasheet (section 9.2.2) for information regarding proper fiber connection.

    You need to have 50 ohm terminations on TD and RD pins with a 0.1uF DC blocking cap.

    Kind regards,
    Ross

    Best regards,

    Ross Pimentel

    Ethernet - Applications Engineer

  • In reply to Ross Pimentel:

    Hi Ross,

    I tried both(50 ohm / 0.1uF cap).
    but, FX Mode is not working.

    When trying to read register 0x0001 Basic Mode Status Register through MDIO the result is 0x7849 which denotes that the link and auto-negotiation bits are off. The LEDs show that the link and auto-negotiation have been completed.

    There is a similar case.
    URL: e2e.ti.com/.../2032488

    But I don't know why read 0x01 register requires two reads.
    Is this a connection to this problem?

    Best Regards,
    John
  • In reply to Yohan Kim:

    Hi John,

    BMSR requires 2 reads because the link bit is latched low for debug purposes. You must always read BMSR twice to see the link status.

    Best Regards,

    Rob Rodrigues

    EFL (Ethernet & FPD Link) Applications Engineer

  • In reply to Rob Rodrigues:

    Hi Rodrigues,

    I tried 2 reads. (BMSR:0x7849)
    but FX not working.

    Is there any other solution?
    Please advise me.

    Best Regards,
    John

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.