This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: DP83848K Reset/X1 pin

Part Number: DP83848K

Dear Sir,

Does DP83848K Reset_N(Pin23) & X1/X2(pin28,27) have build-in as below similar ESD protect structure ?

Thanks!

Steven

1 Reply

  • Hi Steven,

    Yes, there are protection components inside of the DP83848 and the absolute maximum ratings need to be respected so that the components are not damaged.

    Best Regards,

    Rob Rodrigues

    EFL (Ethernet & FPD Link) Applications Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.