Hi,
We have issues with TLK110 PHY(RMII mode) with high-traffic multicast broadcast packets.
The PHY communication stops working(hangs) whenever there is a high-traffic
or when used for long duration(few days). It works normal when there is a low traffic.
The communication was stopping with a traffic more than 4000pps and
after adding PHY software reset command we are able to get the speed upto 20000pps,
but still the communication hangs in between.
Do we have any such related issues with TLK110, which stops working during high-traffic or long run?
Best Regards
Kummi