Other Parts Discussed in Thread: DP83822H, DP83848I, TLK105L, TLK105, TLK106, TLK106L
Please let me know about two points below for DP83822I (or DP83822H) function.
①About datasheet page-65, default value is described "101 1111 1111" and "0x5EE", which is correct?
②Basically, Are DPxxxxx series based on the same internal circuit?
For example, are DP83822I and DP83867's 100 Base-T internal block is the same process? (in addition, ADC/DAC block, etc)
If Yes, is old Ether PHY series (DP83848I) the same process,too?
Best regards,
Satoshi