The datasheet is a bit vague (unless I have missed something) about needed termination for unused pins.
The datasheet states "NOTE: Internal pullup and pulldown resistors on the IO pins are disabled when the device enters functional mode after power up". But in chapter "6.1 Unused pins" it states "DP83867 has internal pullups or pulldowns on most pins. The data sheet details which pins have internal pullups or pulldowns and which pins require external pull resistors".
So how must I terminate JTAG?
And if I strap it to only use SGMII, do I still need to terminate the unused RGMII input pins?
Regards, Jonas